Other Parts Discussed in Thread: TLK105L
Hi,
I have question about Ehter PHY TLK105L.
My customer are using TLK105L on their customer board. When they connected the board(without Power ON) to the Ether Repeater Hub via Lan Cable(straight cable), the LED(LINK LED) on the Hub linked. Because the board power state is off, we don't know why the LED on theHub linked.
The customer also checked with AM437x EVM(IDK) which have TLK105L on the board. The result was same as the customer board. The LED on the repeater hub linked. But this issue doesn't occure when they tried with the other customer board which have LAN8710 on the board(not TLK105L). They captured TD/RD signal of TLK105L side from RJ45 connector. It looks that TLK105L is outputting pulse from TD port. Please take a look at attached file.
This issue occued when they used following Ether Repeater Hub.
Manufacturer: Corega
Model: HUB5PL
www.onino.co.uk/.../corega_hub_5pl_cd_hub5pl.html
By the way, this issue doesn't occure when they used Switching Hub.
Maybe this is TLK105L side issue or maybe not. Is there a possibility with the problem in TLK105L?
best regards,
g.f.