Other Parts Discussed in Thread: DS90UB913A-CXEVM
I have a board design using the DS90UB914A and providing power over coax. I have connected this board to the DS90UB913A-CXEVM and I see the PCLK on my DS90UB914A as a solid 50Mhz. I do not see the LOCK signal go high. There is no data being sent over the link between the boards as I have no camera source for the DS90UB913A-CXEVM. I also do not have I2C access to either part. I am using pull-ups and pull-down resistors on the DS90UB914A to set the modes.
1) If there is no data present over the link, should I still expect to see the LOCK pin go high on the DS90UB914A? As said above, I do see the PCLK output of 50Mhz.
2) I have set the DS90UB914A to BIST mode by tying the BIST pin high. I then set GPIO0 HIGH and GPIO1 LOW for a 25Mhz PCLK. From the datasheet, I would need I2C access to the DS90UB913A-CXEVM to place it into BIST mode, correct? It will not go into BIST mode automatically even if the DS90UB914A is sending BIST data, correct? When set in this mode, I do see the GPO LEDs on the DS90UB913A-CXEVM reflect the status of the GPIO pins. The PCLK output of the DS90UB914A is still 50Mhz in this mode.
My goal is to verify that my new hardware is working and linking correctly to the serializer chip.
Thanks for your help,
Ben Missele