Other Parts Discussed in Thread: DS92LV090A
Hi,
DS92LV090A
When you switch from DRIVER-MODE to RECEIVER-MODE, noise occurs in the differential signal.
What is the reason that noise is generated?
---Detail----
After the signal output to the line side from the system side (differential side) in the DRIVER MODE,
The moment you switch the output to the system side RECEIVER MODE, You can see the noise (width of several ns) to a differential signal.
Detailed procedure of the switch is the following.
①DRIVER MODE (DE = H, REx = H) in the data output to the differential side
②TRI-STATE MODE (DE = L, REx = H) (a few ns) to switching
③RECEIVER MODE (DE = L, REx = L) at the output on the system side
※ During this time, the signal to the line side from the system side is the state that has continued to drive.
※ Once the sandwich the ②, it is because you did not want to make the moment that becomes even momentarily LOOP BACK MODE (DE = H, REx = L).
Best regards