Other Parts Discussed in Thread: DP83620
Hi,
We have developed a board using DP83620 Ethernet PHY and using it for Copper as well as Fiber Ethernet, one at a time. The question I am about to ask is with respect to Fiber Optic transceiver by Apac Opto which is interfaced with this PHY using the application schematic reference given in the TI's PHY datasheet.
The interface is working OK, but I want to know the acceptable/optimal levels of TX and RX signals.
We are using 3.3V for both DP83620 PHY and Optical transceiver power supply.
The following results were taken be referencing RX+/TX+ wrt GND, RX-/TX- wrt GND and then taking difference (CH1-CH2) of the two by using MATH function of the oscilloscope. I had enabled AC coupling mode on the oscilloscope for the measurements. I used two probes in single-ended mode.
TX+: 1.1Vpp
TX-: -1.1Vpp
TX+ - TX-: ~2.2Vpp
RX+: 1.9Vpp
RX-: -1.9Vpp
RX+ - RX-: ~3.8Vpp
Then, I took following measurements by putting probe directly across TX and RX pairs for "kind of" typical differential signal measurement.
TX pair: ~0.98Vpp
RX pair: ~1.74Vpp
I referred the datasheet, but it only gives the following information:
VFXTD_100: 0.5V typ., 0.93V max.
Even the FX_SD voltage levels are not mentioned.
Now, I have two questions:
1) Are my measurements above proper?
2) What are the acceptable levels or ranges for TX and RX signals, Vpp both in single-ended and differential mode, when working with a Fiber Optic transceiver?
Again, the fiber optic Ethernet is working fine on our board, but I am a little skeptical about the levels.
It will be highly appreciable if someone can please help me with these questions.
Please let me know if anything is unclear in my explanation.
Thanks.