This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB901Q - reading address problem

Can you please help with the following problem?
When transmitting command to a slave address (read register) is not transfer bit 0 (read flag). 
To deserializer is sent the address with this bit set (odd number) and 
the serializer send command to slave device with this bit reset to zero. 
(I use the Index ID1 and ID1 Match registers. Values 0x42=camera slave address, 0x82=my reading channel ) Thank very much.