This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVDA1040AQDRQ1 - Vcc



Hi all

Would you mind if we ask SN65HVDA1040AQDRQ1?

<Q1>
The datasheet shows Absolute Maximum Ratings Vcc is -0.3V upto 6V.
In case of the entire temperature range, will it be the same?

<Q2>
The datasheet shows Recommended Operating Conditions Vcc is 4.75 upto 5.25.
If the Vcc is under 4.75V, the device doesn't keep Electrical Characteristics, does it?

Kind regards,

Hirotaka Matsumoto