Other Parts Discussed in Thread: TUSB2077A
Hello,
I am designing a USB hub around the TUSB2077APT and I have questions regarding the enumeration of downstream devices.
For 90% of the time the hub is used it will not be connected to a host (upstream) computer, and the downstream devices will be charging on the hub. The TUSB2077APT is set up for Self-Powered mode without the use of the _PWRONx ports (or the use the _OVRCURx ports).
The question I have is, if there is no host (upstream) computer, will the TUSB2077APT enumerate to the devices attached downstream? The reason for this is the downstream devices are intelligent enough to notice enumeration to an upstream device (host or hub) and choose a higher charging current rate. This is preffered so the downstream devices take a shorter time to fully charge.
Kind Regards,
Phillip