Other Parts Discussed in Thread: SN75DP139, TMDS442
I have an application where I have Displayport++ from the CPU and am using a SN75DP139 (DP++ to HDMI) and TMDS442 (HDMI 1:2) to get HDMI outputs to drive two monitors.
This means I am using the TMDS442 as a 1:2 device and have 3 inputs that are just open. Like to reduce the number of resistors used to terminate all of the unused inputs. Since the 3 input ports will never be used, can I just leave things open or tie them to ground / 3.3 instead of all of the resistors?
So I would like to have my schematic reviewed to answer this question and to see if there is any else that I might have missed.
I would prefer to send the material via email.
Thanks
Tom