Other Parts Discussed in Thread: TLK1501
Hi,
we have two PCBs (A and B) with one TLK1501 each. The PCBs are connected via two optical SFP links. One optical link is transmitting the GTX_CLK from A to B. So both PCBS share the same CLK source.
The second optical link connects the TLK TX and RX and vice versa.
In 80% of cases the connection is establied in both directions (A to B an B to A). (TXD and RXD data is correct)
But in 20% of cases there is a link error. Sometimes there is random data on RXD, sometimes RXD are "high" all the time.
Any suggestions what could cause that trouble. Is there anything to keep in mind during power up?