Other Parts Discussed in Thread: HD3SS460, TPS65982
i,
Do we need to add 2Mohm resistor to GND on SBU signals when using TPS65982? It's suggested in HD3SS460, but not mentioned in TPS65982 datasheet.
Thanks!
Antony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The VESA spec says:
"Figure 3-1 illustrates the system design of a DFP_D on a USB Type-C connector connected to a UFP_D on a USB Type-C connector using a USB Type-C to USB Type-C Cable. The 2MΩ pull-down resistors on SBU1 and SBU2 are representative of the leakage of ESD and EMI/RFI components including termination to ensure no floating nodes, and are intended to show compliance with zSBUTermination in USB Type-C r1.0.
Note: These schematics do not show the ESD protection and EMI/RFI components typically
included in the system designs."
Therefore, the 2MΩ pull-down resistor is not a real resistor, but rather a representation of a leakage resistance. The spec implies that the leakage resistance can also help meet the ZSBUTermination spec in Type-C. If ESD and EMI/RFI components are not used for some reason, zSBUTermination >= 950kΩ is a Type-C requirement.
Please advise your customer to consult the VESA and spec directly, since we cannot post the document online due to licensing. The Type-C spec is public on the USB website.