Other Parts Discussed in Thread: DP83848J, DP83848K
Hello
My goal is to connect an Ethernet PHY (DP83848J) to one of the ports of a KSZ8895 switch. Both components are on the same PCB. Due to this fact I assume I do not need the two transformers (e.g. H1102NL) and I can connect them directly via capacitive coupling. This approach is described in the AN-1519 application note from TI. Have you got any experience with this solution? I am wondering if that is a well-known way of connecting two Ethernet devices and whether there are some limitations which I have to follow?
For example:
What is the maximum trace length of the Ethernet signals when they are coupled by capacities?
Are there some best practice guidelines for the layout design especially about the signal crossover? As far as I know crossing of the signal traces should be avoided. But in case of the capacitive coupling it is necessary because TD+ and RD+ is connected together.
Would it reduce the risk if I would use the transformers anyway? (PHY - Transformator - Crossover - Transformator - Switch)
Or would that make it even worse because transformators decrease the signal quality?
Thank you for your answers.
Yves Willener