Other Parts Discussed in Thread: TPS65982, TPS65982-EVM, HD3SS3212
Hi there, We built in the TPS65982 on our designed board, but there seemed to be problem on charging. Here is the story, I connected the PC board with my Macbook and a USBdrive. When the PC board operated as the Sink, the Macbook can detect the USBdrive and transmit data as well. But the PC board operated as the Source, it can deliver 12 voltage power to Macbook; but the Macbook can't detect the USBdrive, or send data to USBdrive.
Where is the problem? Your Firmware version: TPS65982-EVM_Flash-Image_RTM.BIN
Is there any method to work out? Thanks.