Other Parts Discussed in Thread: DP83640T-EVK, ALP
Hello,
I just purchased the DP83640T-EVK. It seems that Analog LaunchPAD is not communicating with the EVK. Jumper J12 setting on the EVK is set to USB, only the SPEED LED is on, so power seems to be applied?
Installed all drivers for this board. When I launch ALP (v.1.54.0010) on Windows 7/64bit, the board is not detected. Was running the ALPUSBDriver.exe from the /Driver directory, but still no detection of the board.
Is there a setting that I miss?
Thank You.
--Martin