Other Parts Discussed in Thread: TUSB1210, TPD4S012
Hi,
I was trying to do an SI Analysis on the EVM of TUSB1210 EVM .brd file.
Can some one guide me as to which of the buffer model should I use from the IBIS model for the source side and how should I model the USB connector for doing the SI Analysis. I have plugged the ibis model for TPD4S012 but I am not sure as to whether I should use :- TUSB1210_dp/n_hs or the 50ohm_pd model.
How should I model the connector is another doubt that I have? Since TI has made the gerber, I am sure they must have done SI, kindly guide us in that.
Regards