Hello,
We have started layount using DS80PCI800 in 3.3V mode. Can All VDD pins in this mode be connected to one plane as shown in 2.5V mode in figure 14 of the datasheet or just each capacitor should be connected seperately? We also see on the eval board schematic that for both modes this pins are connected together.
Also we would like to know if we can use a 22kOhm resistor instead of 20KOhm for achieving level R in 4-Level input voltage (table 1, page 14 on datasheet)?