Other Parts Discussed in Thread: ISO7240CF-Q1, ISO7241C-Q1, ISO7240C, ISO7240CF
Hi Expert,
According to datasheet of ISO7240CF-Q1/ISO7240C-Q1, ESD protection is defined 4kV (I believe that this spec is Vpeak.).
However, there is no description about RMS(Vrms).
The question is
* Could you show me Vrms for both ISO7240CF-Q1 and ISO7241C-Q1 ?
* Could you show me the time which it can apply Vpeak voltage ?
* Could you show me the time which it can apply Vrms voltage ?
BTW, according to spec of commercial device of ISO7240CF/ISO7240C, Vpeak and Vrms are defined as shown below.
Vpeak : 4000V and can be applied "60s".
Vrms : 2500V and can be applied "1 minute" (but Production tested ≧ 3000V)
Are above spec also applied for Q1 device ?
Best Regards,
Machida