Other Parts Discussed in Thread: SN65HVD1050
Anyone using CAN for automotive applications having or have had issues with bulk current? We are using a SN65HVD1050 on our products and we test to 100mA per ISO 11452-4. We run at 250kBaud and are seeing CAN drop-outs in frequencies <~20MHz. Typically the crash is unrecoverable without power cycle. I have found that other automotive companies (Ford, Chrysler, etc.) start with lower limits and go up to 100mA by 20-30MHz. Is there a documented reason why this is? Does anyone use a different TXR which allows higher testing?