Other Parts Discussed in Thread: ISO3082, ISO3088
I have buit a data rate indipendent repeater as suggested by TI design.
With baud rate of 500k, 32 units load and 240m cable, i place repeater after 120m but it doesn't work.
It works only with short distances. If i omit to place the repeater, and connect the 2 cables together, the line works sussesfully.
Wave shapes seems to be correct, as expected. Line termination resistence is 120ohm at both ends.
I have even tryed the circuit without optoisolation but with same results.
Thaks for any advice.
Enzo Ternavasio