This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS92LV1212A vs DS92LV1210

Hello

It is a performance comparison of the device.

What is the difference between the DS92LV1212A and DS92LV1210?

Best regards

  • Moving to the appropiate forum.
  • Hi Cafain,

    The two parts effectively perform the same function. However, the difference between the two parts is in the Application Information section of the DS92LV121A datasheet:

    "The DS92LV1212A has an improved input threshold sensitivity of +/− 50mV versus +/− 100mV for the DS92LV1210 or DS92LV1212. This allows for greater differential noise margin in the DS92LV1212A."

    In addition to this, the DS92LV1212A has the additional capability of locking to the incoming data stream without the need of SYNC patterns.

    Please also note that the DS92LV1210 is obsolete and the DS92LV1212 are not recommended for new design. Please only use the DS92LV1212A for this situation.

    Thanks,

    Michael