Other Parts Discussed in Thread: TUSB7340
Hello @ all,
i'm using the TUSB7340 in the quite same design as in the EVM Demo-Board.
But when i switch on the power supply, the board will consume 850 mA at 5 V. Further more the TUSB7340 gets very hot.
I think it could be the same problem from the post: e2e.ti.com/.../365370
But unfortunately there is no solution at the end of the post.
Can you help me?
Which informations do you need?
Here is the schematic:
Thank you in advance!
Best regards,
Johannes