This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848CVV RMII and interrupts

Hello

Is it possible to enable interrupts on pin 7 (POWER_DOWN/INT) when the PHY and uC are communicating via RMII mode? is see that the configuration bits are int the MICR and MISR registers so I'm not sure... I would like to get the Energy Detection Control mode to work using RMII if this is possible.

Thanks in advance

Bert