This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848 Load capacitance range at 25MHz



Hi

In Table 7-3 of datasheet, Load capacitance is showed as "Min:25pF, Max:40pF".
But there is the following sentence in 7.3.2 Crystal.
"A 25 MHz, parallel, 20 pF load crystal resonator should be used if a crystal source is desired."

Could you let me know Load capacitance range at 25MHz, please?

Best regards,
Shimizu