Hello
Does the TLK2711 must have its GTX_CLK connected to it in case all I want is to work with its Rx functionality, and I don't need to operate its Tx side at all?
If the GTX_CLK is a must even for the Rx side, please explain why.
Thanks
Amnon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
Does the TLK2711 must have its GTX_CLK connected to it in case all I want is to work with its Rx functionality, and I don't need to operate its Tx side at all?
If the GTX_CLK is a must even for the Rx side, please explain why.
Thanks
Amnon
Hello
I would like please to be sure I fully understood your answer:
1. Does the TLK2711 generates the Rx_CLK already when the GTX_CLK is provided to it even if the Rx link from the far end is not connected at all?
2. At this point (Rx link is in active) the Rx_CLK will be locked on the phase and frequency of the TX_CLK?
3. For the Rx_CLK, will it lock on the far end SerDes CLK already when anything (Comma etc.) will start to appear on the Rx link, or only when Data will appear?
4. To your knowledge, is there a problem with FPGA DCM (timing module) functionality when its input clock (the SerDes Rx_CLK) will change from the local 100Mhz (at power up) to the far end 100Mhz (as data starts flowing)?
5. What is the maximal GTX_CLK frequency difference allowed between the two SerDes?
Thanks
Amnon
Hi Ammon,
Basically, the RXCLK wil be active as long as the TLK2711 is enabled and a TXCLK is present. So, it is up to the device interpreting the received data to monitor the next signals:
RKLSB ==> K-Code indicator/PRBS test results.
RKMSB ==> K-code indicator.
RXD[15:0] ==> Received data bus.
And determine wheter or not the data is valid.
In my unserstanding is no a problem is you change from the local 100MHz (at power up) to the far end 100MHz (data starts flowing) as long as the timing requirements is on spec.
For the frequency tolerance the TLK2711 allows ±100 ppm.
I hope this helps.
Best Regards,
Luis Omar Morán Serna
High Speed Interface
SWAT Team