Other Parts Discussed in Thread: SN75176B, TL431
Hi,
Greetings of the day!!!!
I have been using SN75176 IC for RS 485 over modbus protocol as a slave device. We have installed these devices on multiple locations in industry and it has been observed that the SN75176 IC is failing frequently (say after couple of months). We have used TVS diode array (SM712) as well as MOV's (MOV10D) for protection. But still the IC's are failing not instantly but over the time.
The master device is PLC and maximum 7 nos of slave devices are connected on the bus. Also biasing resistors of 1K and termination resistor of 120 ohm are connected as required.
We have facing same problem on multiple locations. Please guide how to rectify it.