Other Parts Discussed in Thread: TUSB1310, TUSB1310A
You have mentioned in TUSB1310 page "TUSB1310Adevice has SIMILAR FUNCTIONALITY but is not functionally equivalent to the compared device. The TUSB1310A fixes errata found in the TUSB1310 and includes increased functionality but is not pin for pin." My Query is
USB3.0/USB2.0 controller tested with TUSB1310 ,whether the same USB3.0/USB2.0 controller works with TUSB1310A ? Is there is any functional limitations ? If there is any changes required to be made (Pins ,signal) in both sides?