I am using a custom board with a TMS570LC4357 hooked up to a DP83848H. I am unable to read the Phy ID and the MDIO Alive register stays at 0. I am only using the DP83848H in RMII, so all unneeded pins have been left disconnected.
Here are the pins.
MDCLK - 2.34 MHz
PFBOUT/PFBIN1/PFBIN2 - 1.8 volts tied together
X1 - 50 MHz
RESET_N - 3.3 volts
RBIAS - 1.2 volts
I am unsure of what to check next to get this working, is there anything else I should measure?