Other Parts Discussed in Thread: TLK10232
Hello
It's now tested with the following configuration.
■ Configuration
· Case1 (LoopBack)
Board # 1 [FPGA (XAUI) → TLK10232 (10G-KR)] → Cable
↓↓ (LoopBack)
Board # 1 [FPGA (XAUI) ← TLK10232 (10G-KR)] ← Cable
· Case2 (facing)
Board # 1 [FPGA (XAUI) → TLK10232 (10G-KR)] → Cable
↓↓
Board # 2 [FPGA (XAUI) ← TLK10232 (10G-KR)] ← Cable
■ Q1
Therefore, in Case1 and Case2, when carrying out the initialization (Link training, AutoNegotiation, etc.), because the configuration is different, whether you need constraints such as access procedure?
■ Q2
During initialization in Case2, or Board # 1 and the Board # 2 There is a problem to implement simultaneous?
If the problem certain way, the access method used in Case1, like the Board # 1⇒Board # 2, is scheduled be conducted in order.
Thank you will please more.