Customer want to use SN65LBC180A of Half-duplex operation.
Is there a way of Half duplex circuit?
【Additional information】
・Customer was using SN65LBC180A (Full duplex).
Suddenly, latest board must operate Half duplex.
・Customer request is 2-way following
①Half duplex RS485 that Pin compatible with SN65LBC180A.
② If ① nothing, using SN65LBC180A on Half duplex.
(Is it OK for Y-A and Z-B short?)
・Z-pin and Y-pin is open
Best regards,
Satoshi