Other Parts Discussed in Thread: ISO3086
Dear Technical Support Team,
I have a question about ISO3086.
Do you have a specification of VOA/VOB?
I'd like to know about it, but I can't find it on datasheet.
I think that I can calculate the spec from VOD and VOC.
Is following calculation correct?
I refer to "Figure 12. Test Circuit and Waveform Definitions For The Driver Common-Mode Output Voltage".
<Calculation for VOA / VOB>
■MIN
VOA = 1V+0.75V = 1.75V
VOB = 1V-1.15V = -0.15V
■TYP
VOA = 2.6V+1.15V = 3.75V
VOB = 2.6V-1.15V = 1.45V
■MAX
VOA = 3V+1.15V = 4.15V
VOB = 3V-0.75V = 2.25V
<datasheet spec>
|VOD|: MIN 1.5V / TYP 2.3V(RL=54Ω)
VOC: MIN 1V / TYP 2.6V / MAX 3V
Best Regards,
y.i