Hello Everyone,
In one of our project, two boards are kept at a distance of 1 meter and has 12 digital signal lines(3.3 V,LVCMOs) connected between them.Out of these 12 lines, few are clocks, few carry asynchronous data and maximum clock rate is 6.75 Mhz. In order to reduce the number of lines running between the cards, we are planning to use, SERDES IC so that 12 signals can be mapped on to 2 differential line. Kindly let me know,
1.Is using SERDES is the right approach ? if yes which device I can use?
2. Disadvantages of SERDES.
Thanks & Regards,
Mamatha