Other Parts Discussed in Thread: SN65HVD1040
I am looking at the SN65HVD1040 data sheet and noticed a peculiar spec. The Recommended Operating Conditions show only a Junction temp of 150°C and the rest of the specs are defined as over recommended operating conditions. The Absolute Maximum Ratings list the Junction temperature of -55 to +170°C but the Storage temperature of -40 to +125°C temperature. This implies that you can run the part hotter than the max Storage temperature. There is a note in the Description section (5) that the part is characterized for operation from -40 to +125°C but that is not reflected in the parameter tables.
I am looking for a CAN transceiver that can go to low power and still monitor the lines for wake-up on CAN activity and the design will to run up to 130°C. Does this part run at over 130 C, or is there a different part that will? Thank you very much.
Russell