Other Parts Discussed in Thread: LMH0307, LMH0303
Termination Fault detection is not proper in default setting of the SDI cable driver[LMH0307].
Setup used and testing procedure as follows:
Hardware connections are as given in reference schematic in datasheet.
Input 700mv Pk-Pk.[HD SDI signal]
Output Connector is 75ohm with 75ohm BNC cable.
Testing in default condition :
always showing termination fault.
After changing HD threshold value of all channels to Maximum, Differential channels[SDO bar] were able to detect Termination fault properly.but other channels are not detecting termination fault.
After reducing the Amplitude to lowest value Normal channels [SDO] are detecting termination fault properly but differential channels are now continuously showing no termination fault.
Kindly suggest how we can resolve this issue.As we will be monitoring the fault conditions periodically.