Other Parts Discussed in Thread: TPS65982, TPS2544, TPS2514, TPS2513
Hello,
If We are using TPS65982 for charging of USB Type C based device and do we need to connect D+ and D- pin of USB type C connector to any other BC 1.2 specified IC(like TPS2513/TPS2514) for charging of USB 2.0 based devices?
As we know that we can use USB Type C to USB 2.0 micro USB cable for charging of USB 2.0 devices. As per the datasheet page number 53 ofTPS65982 "Battery Charger (BC1.2) Detection Block" point, it mentioned it can detect the BC1.2 devices so can we say that it will support for charging of all USB 2.0 based devices?
If any other IC are available for both use case then please suggest us.
Any help in this case should be appreciated.
Thanks,
Chetan Panchal