Other Parts Discussed in Thread: TPS65982
Hi Team,
my customer has a question about the PP_5V0 current limit setting, if their PP_5V0 maximum current limit is set to 3A, per the below table, which setting # will be automatic set by TPS65982 digital core? Note, the table has the MIN, TYP, MAX value, we are not sure how the TPS65982 digital core algorithm will do for the setting # ? for example, for the setting 12, is that meant when the load current is exceed to 3.075A, the current limit protection will possible to be activated? Please advise. Thanks.
Regards,
Arthur