Hi,
we are looking for a better understanding of the distance that can be reached between camera sensor and host.
the LVDS324 is designed to interface to a set of camera sensor output Aptina HiSPi, Sony LVDS, and these sensor are for example AR0331, AR0330, AR0132, MT9M024.
I we assume that the sensor is operated at lower framerate and the Pixel Clock is 75MHz, or 37.5MHz. Given the 4-lane LVDS being used with the LVDS324, is there an estimate of the distance between sensor and host, that could be achieved with this technology?
Thanks,
--Gunter