Other Parts Discussed in Thread: DP83867IR
The DP83867IR datasheet(SNLS484B) describes the 4-level Strap Resistor ideal values in Table 2. These values do not consider other circuit except the strap circuit. If a device connected to a strap pin has internal resistor, the internal resistor value of the strap pin must be considered.
All strap pin are PD (internal pull-down). What is the internal pull-down resistor value of each strap pin?
When VDDIO=1.8V, what is the voltage range to select each mode?
Best regards,
Daisuke