Other Parts Discussed in Thread: TUSB8041
Hi,
I am using TUSB8041 for connectivity of my system. I am using 3 out of 4 ports for communication and 4th port is kept unconnected would be used in future. System is configured to full power management control and individual control power management enabled.
On port1: I am connecting a USB2.0 device which is not powered from VBUS(externally powered device). So there is only dateline (d+ and d_) is connected. Rest USB 3 pins are not connected. All lines are hardwired in PCB and no connectors for this port. The power management pins are also not required. Can I leave PWERCTL1/BATEN1 unconnected? or Should I ground it? And how about Overcur1z? Currently I am planning to connect to Vdd to keep it active high.
FYI: On port 2 and 3 I am using power switches to control the downstream power and on port 4 all the pins are unconnected. On port 2 and three there would be USB 3 micro B connectors.