Other Parts Discussed in Thread: SN65HVD1781, SN65HVD1786, ISO3088
Hi,
I'm starting off a new design based on the RS485. I think the SN65HV1786 (5Vcc power supply) and (3.3V Power Supply) is going to be a good option because they have fault-protection. But I need some question before to read the datasheets.
Are these RS-485 transceiver fail-safe? Is necessary to put these resistors Rfs?
And I've got another question. If I use only a master and a slave in a bus RS-485. Can I eliminate the RT1 and RT2 resistors? I am using point to point connections of around 1 meter in length.
Thank you so much. Best regards.
SN65HV1781