Other Parts Discussed in Thread: TMDS141
I have a scenario where the TMDS141 is driving DC-coupled into a chip that wants to see common mode voltage at 0.7V, running at 2.25Gbps. There are 50 ohm pullups to 3.3V on the outputs.
If these external resistors and rail are changed to produce the desired common mode voltage, and RVSADJ is used to control swing, can this be made to work?
I think we have the freedom to make these changes, since the bus is entirely isolated on the board, so it just needs to be made to work.
Using weaker pullups is a no-brainer change, but the pull-up *rail* would be more difficult to change.
Thanks!