Hi,
I'm thinking about using this RS-485 isolated transceiver. And I would like to know approximately the power consumption working to a speed of 1Mbps. I'm not sure If I'm reading well the datasheet.
According to the page 7/31 [8.7 Supply Current].
Icc1 [Vcc=3.3V] MAX = 8mA
Icc2 [Vcc=5V] MAX = 10mA
Then Total Power = 3.3*8 + 5*10 = 76.4 mWatts. Is it correct?
Thank you so much. Best regards.