Other Parts Discussed in Thread: PCA9306
Hi,
DSD90UH949-Q1: On our board the DDC-IF is used only internal so it doesn't has to fulfil the HDMI-Spec. We've plugged the I2C-IF and the DDC-IF together with an I2C master to a 3V3 bus.
Question:
1.) how are the threshold voltages for VIH, VIL and VOH defined? (e.g. VIH = 0,7*VDD, VIL = ...)
2.) to which supply voltage are the threshold related to? (e.g. voltage supplied at RX_5V, ...)
3.) when connecting the DDC and I2C ports together, is it allowed to supply "DS90UH949/pin43 = RX_5V" with 3V3 to meet the threshold requirements?
Thanks in advance
Thomas Sagcob