Other Parts Discussed in Thread: SN75LBC172
Dear Technical Support Team
I have a question about SN75LBC172.
Following is a waveform on Osillospcope.
Y and Z drive high(between cursole X1 an cursole X2) at the same time after an enable(Gn) is high(Enable(G) tied GND).
After that these levels fall down slowly and keep immideately dividing voltage level(①:2.78V / ②:2.22V) depended on register
Is it the correct operation for Y and Z?
I think that Y and Z are Hi-z and these volatage shows immideately dividing voltage level(①:2.78V / ②:2.22V).
5V - 390Ω- 100Ω- 390Ω- GND
↑ ↑
①Y ②Z
Best Regards,
y.i