A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI , Under 2-lane FPD-Link III mode , if user connect the high-speed cables as DOUT0x to RIN1x , DOUT1x to RIN0x ( If operator will fail), does the device can send data or not ? (Does the device detect the failuer and will be able to correct ? )
If the 947-948 are assumed, the data can come out when the cables are connected DOUT0x to RIN1x or DOUT1x to RIN0x. The 947 has an auto-detect if the ports 0/1 are swapped.
Did you assume the 947-948?