Other Parts Discussed in Thread: DP83867IR
Hello.
Please help about LED state of DP83867ir.
The customer uses three LED signals by default setting.
(LED_0, LED_1, LED_2, p.70, p71) of the manual)
Think that LED_1, LED_2 shows the state of the link
Therefore, these LED thinks that LED turns off the light when they pulled out Ether cable.
The setting of auto negotiation renews a register to become enable.
And set it so that LED works in the state that link negotiation was made.
link negotiation is in a made state, and work as I thought of.
In contrast, two LED may have worked when they pull out Ether cable.
What kind of situation will be supposed?
In addition, became 0 about bit2 of BMSR(0x0001).
Can guess that this is in a condition that a link is not made?
Though a link is not made, will be that LED_1, LED_2 has flashed?
The effect of the MAC signal?
Depending on a state of the MAC side, will a thing becoming in a state such as the above be thought about?
(e.g., a clock about state transition of the LED output which clocks such as RGMII are not supplied to is not input)
Regards.
k-hashi.