Other Parts Discussed in Thread: DP83848I, DP83848I-MAU-EK
Hi,
I am currently working on a project with a DP83848I Analog Evaluation Module PHY connected to a PIC32MZ2048ECG100 microprocessor (in the form of a Digilent chipKIT Wi-FIRE) as a MAC. However, accesses to the PHY registers using the software inside the PIC32 return 0x0000FFFF (or all ones) regardless of which register I attempt to read. The PHY is strapped at Address 1, connected in alternate configuration + MII mode. All the defaults are enabled on the PHY.
Furthermore, attempts to send a ping to the microprocessor lead to timeout. The LINK LED is active on the DP83848 module, but the ACT remains off. A loopback cable also does not light up the ACT LED. Is there a way to check the registers of the PHY itself externally, and also to see if it is communicating properly?
Thank you for your help.
Regards,
Rush