This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVPE502B input impedance

Dear Specialists

My customer has a problem of unconnecting to USB2.0.

He is concerned the spec of input impedance between SN65LVPE502B and EZ-USB FX3(cypress).

He confirmed cypress and got answer.

Could you please see listed below and advise.

Is there any problem in SN65LVPE502B?

--------the answer from cypress--------

This is a compatibility problem between FX3(CYUSB3014) and SN65LVPE502B.

The issue is with the impedance range that the redriver uses when USB 3.0 is disabled.

FX3 will use any impedance value under 150 ohms as a valid super speed impedance, and get into compliance state.

USB spec says impedance under 30 ohms is valid, and USB 2.0 only links should have impedance above 20 K.

There is no description of what should happen between these ranges.

We are using 150 ohms as our threshold.

--------end of answer--------

I appreciate your great help.

Best regards,

Shinichi