Other Parts Discussed in Thread: TPS65982
Hi,
I can not use SRDO command to send the RDO data from sink to source to change the delivery power.
After the SRDO 4CC command is sent, I use the Data1(0x09) to read two byte data and it get 0x40 0x03 always such that I cannot send the RDO data by Data1(0x09) command. From the Python Script example, the data send by Data1 command seem to make sure the two byte data read of Data1(0x09) is 0x40 0x00.
Please give me the flow or condition to use the SRDO command.
Best Regards
Philip Jou