This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7240M vs. ADuM1400 - supply current of 90Mbps, 50Mbps

Guru 20090 points
Other Parts Discussed in Thread: ISO7240M, ISO7340C, ISO7640FM, ISO7840

Hello,

Could you please let me know the maximum supply current of ISO7240M at the following conditions?

-Data Rate : 90Mbps, 50Mbps, 25Mbps
-Vcc1=Vcc2=5V

I promoted the ISO7240M for replacment the ADuM1400
If the ISO7240M supply current is smaller than ADuM1400, they may use our device.
ADuM1400 has the 90Mbps supply current on the EC table.
Regarding ISO7240M,  I can see the supply current curve but there is no 90Mbps data.
And they use the ADuM1400 for 50Mbps, 25Mbps.


Best Regards,
Ryuji Asaka