Other Parts Discussed in Thread: TUSB8041, TUSB9261
I am currently working on a device which will mount to the back of a Microsoft Surface Pro 3. This device will extend the capabilities of the Surface by providing 3 additional USB 3 ports using the TUSB8041 and also by providing additional storage using a SATA Solid State drive connected via the TUSB9261.
The Surface Pro only has one USB port. This means that I will have to connect the TUSB9261 directly to one of the downstream ports of the TUSB8041. Are there any recommendations for interfacing 2 USB 3 on the same PCB without the use of traditional USB connectors?
To make my request clear, I want to have both the TUSB8041 and the TUSB9261 on the same PCB. I want to connect the upstream port of the TUSB9261 to one of the downstream ports of the TUSB8041 on the PCB.
Are there any special termination considerations? Do I just route the traces as I normally would when using the correct connectors, but instead just place traces instead of connectors? Are there any impedance considerations? Is this a bad idea altogether? Are there other ways of accomplishing this without having 2 boards for these 2 chips?
Any guidance is MUCH appreciated!