Other Parts Discussed in Thread: SN65HVDA100
Hi,
my customer is asking following question:
‘’I would like to use the SN65HVDA100.
The microcontroller I am using has a UART which only can generate 8,7 or 6 bit data words.
For the LIN bus the "break field" should have 13 bits. I have noticed the SN65HVDA100 outputs the same signal on the LIN bus as I generate on the UART side.
Is there any standard way of generating the "break field" with 13 low bits for the Lin bus with the SN65HVDA100?
I would think most of the UARTs on the microcontroller side cannot generate the 13 bits."
Thank you for any recommendation.
BR Martin